WILMINGTON, Mass. (PRWEB) January 19, 2021 ― Heilind Electronics, a leading global distributor of electronic components and authorized distributor for Panduit, has expanded its labeling and identification portfolio solutions with the addition of Panduit’s MP100 and MP300 mobile printers. These printers combine printing technology from Epson with industrial labels and application knowledge from Panduit, resulting in exceptional capabilities, print quality, speed and ease of use.
The MP100 prints continuous labels from mobile labeling apps and is compatible with Bluetooth, Wi-Fi and USB. This model offers label widths up to 1 inch and an automatic cutter. The Panduit MP300 prints 360 dpi die-cut and continuous labels up to 1.5 inches wide and features a 1.4 inch per second print speed, an automatic cutter with full or half cuts, USB connectivity and a rechargeable battery pack.
Both printers work with Panduit’s fast-loading label cassettes, which include patented Turn-Tell labels that rotate for easy visibility. The printers provide self-laminating adhesive labels for wire/cable identification, as well as flat labels for signs, pipe and voltage markers and more.
These new printers integrate with Panduit’s Easy-Mark Plus labeling software, making it easier to manage all Panduit printers from one computer.
The MP100 and MP300 mobile printers from Panduit combine best-in-class print technology with industry-leading labeling and software capabilities. This makes them ideal for use in electrical and network environments, from the data center to the telecom room and the jobsite to the plant floor.
Visit Panduit’s MP100 and MP300 mobile printers page for more information.
About Heilind Electronics
Heilind Electronics, Inc. is one of the world’s leading distributors of connectors, relays, sensors, switches, thermal management and circuit protection products, terminal blocks, wire and cable, wiring accessories and insulation and identification products. Founded in 1974, Heilind has locations throughout the U.S., Canada, Mexico, Brazil, Germany, Singapore, Hong Kong and China.
About Panduit
Panduit manufacturers a broad selection of wire harness, heavy duty cable management and control panel solutions that help customers meet design, quality and regulatory requirements in a timely and cost-effective way. With automated tooling, technical support and worldwide availability of quality products, Panduit is a single-source partner to help you organize, connect and protect electrical and mechanical systems.