JAE JN1V/JN2V Series Waterproof Circular Connectors

The JAE JN1V/JN2V series come in the same form factor and dimensions as their popular traditional JN1/JN2 series. The five-point contact structure of this new series has been upgraded to improve the reliability under higher vibration. The connectors can withstand 245m/s2 (25G), which is 2.5-times higher shock and vibration compared with the conventional JN2 series. The JN1V/JN2V series can be widely used as a compact waterproof I/O connector for servo motors for robots, automation machines, machine tools, and other industrial equipment. Please note that the new plug will mate to the traditional JN1/JN2 series receptacles.

  • Superior contact reliability achieved with a five-point contact socket contact with high vibration resistance
  • Compliant with 245 m/s2 (25G) vibration conditions
  • Designed to mate with standard JN1/JN2 receptacle connectors
  • Utilizes same semi-automatic crimping tool (applicator) as JN1/JN2 contacts (Requires manual crimping tool exclusive to JN2V)
  • One-touch, push-and-twist, lock mechanism
  • IP67 rated dust and waterproof (when mated)
  • The right angle plug can be set in different 90 degree increment cable orientations
  • JN1V is an all-plastic type, and JN2V is an robust type partially using metal parts
  • Industrial (non-Robotics)
  • Computer / Datacom / Telecommunications
  • Contract Manufacturing
  • Servo motors
  • Semiconductor manufacturing equipment
  • Communication equipment
  • Measurement
  • Industrial equipment such as robots, automation machines, and machine tools which all require vibration resistance and waterproofness