Amphenol Times Microwave Systems
Amphenol Times Microwave Systems is a leader in coaxial transmission line technology and production serving military, aerospace, wireless communications and industrial applications. Their engineering expertise combined with a range of manufacturing capabilities in the US and China, Amphenol Times Microwave Systems addresses both specialized applications with extremely demanding performance requirements and high volume commercial applications at frequencies from several KHz to 50 GHz.
A division of Amphenol Corporation, Times Microwave Systems is division of one of the largest manufacturers of interconnect products in the world. Amphenol designs, manufactures and markets electrical, electronic and fiber-optic connectors, interconnect systems and coaxial and specialty cable.

Amphenol Times Microwave Systems is a leading solutions provider in the telecom industry, offering a comprehensive range of high-performance coaxial cable products and accessories designed to meet the demanding needs of modern telecommunications infrastructure. Their flagship LMR® Series provides low-loss, flexible, and durable cables ideal for both indoor and outdoor applications, including wireless systems, antenna feeder runs, and in-building communications. With a focus on reliability, ease of installation, and compliance with industry standards, Times Microwave Systems delivers robust solutions that ensure efficient and long-lasting signal transmission. Supported by a global distribution network and expert technical assistance, they are a trusted partner for telecom providers worldwide, enabling the deployment and maintenance of critical communication networks.
Featured Products
LMR®cables are high performance broadband, flexible, low loss 50 Ohm coaxial communication cables designed for use in wireless applications such as:
- Internal component and equipment wiring
- Inter/intra cabinet jumpers
- Base station and antenna jumpers
- Tower and pole feeder runs
- In-building runs, including riser runs and air-handling plenums
- Rooftop installations
- Oil & Gas Fields
- Power Plants
A full range of LMR®cables are available from LMR-100 (0.100″) all the way up to LMR-1700-DB (1 1/4″).
- LMR-FR: Fire retardant cable for installation in building vertical risers or where fire retardancy is critical, both UL and CSA listed (CMR/CATVR).
- LMR-LLPX: cables are the most rugged and easiest to install plenum rated cables available, especially for difficult installs in older buildings. Cables are both UL and CSA listed (CMP/CATVP).
- LMR-DB: Watertight cables with an inert flooding compound injected in the braid to completely eliminate the possibility of any water migration with a 10 year warranty! The DB feature is optional on sizes 600 and smaller, and standard on sizes 900 and larger.
LMR® Ultraflex: Stranded center conductor and thermoplastic rubber jacket for maximum flexibility.
- LMR-75: These are 75 Ohm versions of the standard LMR cable for unsurpassed performance in broadband video and specialized RF applications.
Amphenol Times Microwave Systems designs rugged, simple to use termination tools for LMR®cables. Amphenol Times Microwave Systems offers a large set of crimping tools ranging from economically priced tools for small jobs to very rugged ratcheting crimp handles with insertable hardened dies for all LMR®cable sizes. These tools make the termination process so easy you can do it blindfolded!
Amphenol Times Microwave Systems LMR®Hardcase Tool Kit: The LMR® Tool Kit contains all of the tools required for a specific job all in one place. This new hard case tool kit with hard foam cut-outs for LMR-195, 200 and 240 goes a long way towards addressing the challenge. This is the first in a series of hardcase kits which will keep all of the tools required for a specific job all in one place. The included tools include the CT-240/200/100 crimp tool, the CST-195/200 prep tool, the CST-240A prep tool, and the CCT-03 cable cutting tool.