TE Connectivity
TE Connectivity Ltd. is a $14 billion global technology and manufacturing leader creating a safer, sustainable, productive and connected future. For more than 75 years, TE’s connectivity and sensor solutions, proven in the harshest environments, have enabled advancements in transportation, industrial applications, medical technology, energy, data communications and the home. With 80,000 employees, including more than 8,000 engineers working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS.
Increasing the durability of technology requires connectivity solutions engineered for reliability. TE Connectivity ruggedized connectors, sensors, and more are designed to optimize the throughput of data, power, and signal – while improving tolerance in systems continuously exposed to extremes such as vibrations, temperatures, voltages, pressures, and moisture.
With TE’s accelerometers, you can accurately measure vibration and motion in heavy-duty equipment operating in harsh environments. Their heavy duty connectors are designed to provide reliable power and signal transmission in rail systems, robotics, and construction machinery. And with their AMPSEAL connectors, you gain a rugged, environmentally sealed cable-to-board solution, manufactured to withstand high-temperatures and harsh conditions.
Together with Heilind Electronic’s extensive TE Connectivity inventory, you are sure to find connectors, relays, switches, circuit breakers or any other item you are likely to need for your applications.
Featured Product Lines
Connectivity Solutions for your HVAC System
It’s not easy being an HVAC system… whether installed in a home or a commercial building. HVAC systems are exposed to harsh environments ranging from extreme heat to frigid temperatures — both inside and outside the system.
The components in your design must withstand dust, debris, thermal shock, condensation, humidity, and corrosion. Choosing weak components can reduce energy-efficiency and degrade the system’s performance. Learn More
TE Connectivity offers advanced automation solutions to optimize warehouse efficiency, focusing on reducing downtime and streamlining operations. Their sensors, connectors, and components are designed for reliable performance in modern warehouses, seamlessly integrating with robotic systems like AGVs and pick-and-place robots. These solutions improve inventory management, order fulfillment, and operational accuracy while enabling faster decision-making and reducing human error. Built for durability, TE Connectivity’s products help lower maintenance costs and enhance productivity, allowing businesses to stay competitive in fast-paced industries. Learn More
FEATURED PRODUCTS
Reliable Protection in Harsh Environments
Heat shrink tubing from TE Connectivity (TE) offers reliability and protection of critical components in the most demanding applications and the harshest environments, including chemicals, moisture, water, abrasion, high temperatures and fungus. TE’s heat shrink solutions help manufacturers avoid countless design requirements to meet rugged and performance demands, as well as new challenges brought on by ever-changing market trends and evolving market needs.
Heat Shrink Tubing offers:
- Highly flame retardant, able to withstand extreme temperature change. Operating temperature ranging from -55°C up to 150°C
- Increased safety enabled by tubing color differentiation which helps identify battery poles and vehicle power type
- Flexibility allows for quick and easy installation, enabling faster production ramp-up
- Seals & protects against mold, debris, and moisture – preventing corrosion
Relays for Every Application
Our extensive variety of relays includes low-signal, mid-range, high-voltage, crystal can, and solid-state. We also offer TE protective and time-delay relays, which not only withstand extremes in temperature, shock, vibration, and altitude, but conveniently combine multiple functions into a single package.
Included in our portfolio are TE’s AGASTAT, CII, HARTMAN, KILOVAC and Potter and Brumfield relays ― some of the most respected brands in the high-performance switching industry.
TE Sensor Solutions
TE Connectivity’s innovative technologies enable measurement capabilities in industries like automotive, industrial, medical, aerospace & defense, appliance, and transportation. Our TESS portfolio includes both out-of-the-box and custom solutions.
These products are at the heart of everyday applications and measure properties such as flow, fluid property, force, humidity, photo optic, piezo film, position, pressure, scanning, temperature, vibration, and ultrasonic. Harsh environment options are also available.
TE Connectivity manufactures an extensive range of products from hand tools up to fully automatic machines for wire and PCB applications. Having a quality connection is essential to delivering high performance and reliability in extreme environments. From crimping a terminal onto a wire or pressing a connector onto a board, TE’s tooling equipment are designed to maximize production uptime, extend tooling life and minimize manufacturing waste. Download the TE Application Tooling line card to learn more.
Browse All TE Application Tooling
TE’s complete line of quality application tooling solutions include:
- Portable wire processing
- Applicators
- Semi-automated wire processing
- Heat shrink machines
- Magnet wire equipment
- Board processing equipment
With the emergence of the Internet of Things (IoT), the system of uniquely identified interconnected devices that are enabled to transmit and share data over wireless networks, technological advances are needed to create a safer, sustainable, more productive and connected future. As IoT growth has been fueled by technology, it also has been facilitated by the strength of other technological advancements.
Antennas are critical to transmitting and receiving radio frequencies (RF) and along with filter and power amplifiers, must work adeptly with fiber optic and cloud-based technologies. They must also enable near limitless wireless connectivity between devices and databases, while at the same handle high-power signals and operate within stringent thermal
conditions. These are functionalities all critical to the development of an IoT application and performance of a smart environment.
Antennas play a complex role in the dynamics of the IoT. As IoT ecosystems move to support high-density, low latency networks and continue to incorporate various new features into radios and overall system layouts, there is an even greater premium put on antenna system design.
View the following antenna solutions that are an integral component in the creation of IoT applications:
- Standard and Custom Antennas for IoT
- Wi-Fi 6/6E Triple Band Antennas
- Emergency Service MiMo Antenna
- Light Transit Low-Profile MiMo Antenna Range
- MiMo Rooftop Antenna
Download these brochures for more information:
DEUTSCH Mil-Spec Connectors
TE’s DEUTSCH line brings you the combined expertise of TE Connectivity and DEUTSCH in a total interconnect solution, including military specs such as the MIL-DTL-38999 DEUTSCH connector series.
Included in our DEUTSCH line of connectors is the DMC-M Series: a rugged modular solution for aerospace connectivity. DEUTSCH DMC-M Series connectors are designed to provide flexibility through the mixing of male and female modules in each connector half. These compact, lightweight connectors are EN4165-compliant and available in both multi-cavity and single-module configurations.
Deutsch TE Connectivity
TE DEUTSCH Products Include:
- TE DEUTSCH D38999 Connectors
- TE DEUTSCH 369 Series
- TE DEUTSCH M83513 Micro-D Connectors
- TE DEUTSCH M39029 Contacts
Potter & Brumfield Solid State Relays SSRDC Series
TE Connectivity’s (TE) Potter & Brumfield Solid State Relays SSRDC Series utilizes DC switching technology with low power dissipation FETs which includes optical coupling. The SSRDC Series is used in DC load applications, which provides reliable DC switching up to 40A and operating voltages up to 200V. Heat sink mounting to maintain base temperatures and load conditions, is recommended
Benefits
- Provides low power dissipation to extend electrical life
- Achieves high Pulse Width Modulation with low switching times when providing power to devices
AS85049 (M85049) Adapters & Band Straps
Made to NAVAIR standards, TE Connectivity’s AS85049 (M85049) adapters and band straps can be used with D38999 and most other military circular connectors. These termination solutions are applied to the back of connectors for shielding, screening and grounding to cable harnesses – ultimately enhancing EMI/RFI protection. Band straps include M85049/128 part numbers.
- Side-entry straps for easy installation and repair
- Self-coupling locking nut for improved vibration resistance
- Wide selection of sizes, materials and platings
- Aluminum body with cadmium or electroless nickel plating
- Adapters offered in straight, 45°C and 90°C configurations
- Used in marine, aerospace, military ground vehicles, space based systems and more
Featured Digital Datasheets
Featured Digital Datasheets
Harsh environment connectors feature several design elements to help protect connections as they deliver power or data reliably. These features include durable contacts, IP rating for dust and water, rugged metal or thermoplastic shells, watertight seals, and a firm, secure locking mechanism. But what option is best for your application? Download this informative white paper to learn your options when selecting a ruggedized connector.
Topics covered include:
- What conditions rugged assemblies designed to withstand
- Options to protect against dirt and water ingression
- Design options in specifying a rugged connector
- Cable assembly option
When developing sensification systems for personal healthcare, monitoring, and diagnoses, designers need to consider many factors that contribute to the integrity of a sensed signal and to the ability of a system to operate reliably, regardless of the environment. Download this white paper to learn what factors are necessary to create systems capable of executing upon the promise of personal healthcare.
Topics include:
- Core components of the sensification system
- Design requirements for the sensification system
- How terminals, connectors and sensors play a key role
- Performance requirements throughout the design process
Learn how TE Connectivity’s heat shrink tubing solutions are designed to help ICT manufacturers meet a wide range of needs and condition in this informative white paper.
Experience our whitepaper on 3D printer design, featuring discrete wire, FPC/FFC connection and ribbon cables and learn how these products and more can take your 3D print design to new levels. Get an inside look at a printer and all the parts that help it maintain functionality. We will focus on answers to questions such as how to make the most sufficient design for a particular end product, and how to move from power to the control to subsystems. How are all these subsystems synched together? How does the printer interact with the user is it through a touchscreen, switches, or other inputs? How does it interact with the outside world through Wi-Fi connectivity?
The subject device of the teardown is a consumer desktop 3D printer broken into five main categories:
- Power supply
- Main control board
- Print head carriage
- X, Y, Z access control
- Print stage
TE Connectivity Press Releases
TE Connectivity, TE, TE connectivity (logo), and EVERY CONNECTION COUNTS are trademarks of the TE Connectivity Ltd. family of companies.